IPC - follow the Application Note and API, or the multicore sample code?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IPC - follow the Application Note and API, or the multicore sample code?

964件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by g_mocken on Tue Jul 22 01:57:45 MST 2014
I am currently investigating Inter Processor Communication. I have read the Application Note 1117 and looked at the mc_sa_blinky sample code, too.

The AN1117 dates back to 2012 (and FreeRTOS v7.x), while the sample code appears to more recent. The sample code does not make use of the well-documented API defined in AN1117.

So what is the recommended route to follow? What's still supported and what is deprecated?
ラベル(1)
0 件の賞賛
返信
0 返答(返信)