IEC60730 library for LPC804

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IEC60730 library for LPC804

1,425 Views
grzegorzkonopko
Contributor III

Dear

Does NXP provide provide IEC60730 library for LPC8xx family?

Or any similar self testing routines.

/Greg

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,280 Views
soledad
NXP Employee
NXP Employee

Hi, 

Unfortunately, there is no IEC60730 library or similar for LPC8xx family.

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply