IEC60730 library for LPC804

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IEC60730 library for LPC804

1,439件の閲覧回数
grzegorzkonopko
Contributor III

Dear

Does NXP provide provide IEC60730 library for LPC8xx family?

Or any similar self testing routines.

/Greg

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,294件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi, 

Unfortunately, there is no IEC60730 library or similar for LPC8xx family.

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信