IEC60335 certificate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IEC60335 certificate

1,944件の閲覧回数
tomi
Contributor I

we are using LPC1768 in a safety project.

there is a Application Note AN10918 for IEC60335 Class B certified library  

where can i find the certificate for this library

Thanks for help

Thomas

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,796件の閲覧回数
arunt
Contributor I

Does the LPC800 have a library for IEC60355?

0 件の賞賛
返信

1,796件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the Sec_121512 doc attached. 

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信