IEC60335 certificate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IEC60335 certificate

1,985 Views
tomi
Contributor I

we are using LPC1768 in a safety project.

there is a Application Note AN10918 for IEC60335 Class B certified library  

where can i find the certificate for this library

Thanks for help

Thomas

Labels (2)
0 Kudos
Reply
2 Replies

1,837 Views
arunt
Contributor I

Does the LPC800 have a library for IEC60355?

0 Kudos
Reply

1,837 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the Sec_121512 doc attached. 

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply