ICSP/JTAG INTERFACE LPC23xx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ICSP/JTAG INTERFACE LPC23xx

2,105 次查看
angel08
Contributor I

Hi good day! I would like to know which programmer I need for programming a LCP2366 using the following interface: 

angel08_0-1681313377402.png

I was trying with a JLINK because I can see in the segger website that jlink is useful for LPC23xx mCUs

angel08_1-1681313446520.png

But, with the Jlink, I don't have the ISP_Request, J1587-TX and J1587-RX signal, so, maybe I need an adapter for using JLink, but I don't know which

 

ISP_Request signal is P2[10]/EINT0

J1587-TX signal is TXD0

J1587-RX signal is RXD0

 

Please, could you support me? Thank you

标签 (2)
0 项奖励
回复
1 回复

2,087 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As you know that the LPC23xx was a product before the NXP spun off from Philips, it is very old.

I suppose that you can use Keil tools to download code and debug with JTAG interface using ULINK 2 device.

xiangjun_rong_0-1681355413690.png

 

In ISP mode, you can use FlashMagic tools to download code with uart interface.

This is flashmagic tools link:

https://www.flashmagictool.com/download.html&d=flashmagic

 

Hope it can help you

BR

XiangJun Rong

 

 

0 项奖励
回复