IAP runs into hard fault

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IAP runs into hard fault

640 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Alex on Fri Oct 10 07:00:29 MST 2014
Hi,

I'm using a LPC1776 at 120 MHz clock frequency.
I like to erase a sector of the internal flash via the IAP interface but when I try to call the IAP handler to prepare the sector for write/erase operation a hard fault is raised.
I performed a test with 80 MHz clock frequency and it performed quite well.
Does the boot rom have a clock limitation?

Another thing is that the earse handler always returns busy @ 80 MHz clock. What may the reson be?

regards,
Alex
标签 (1)
0 项奖励
回复
0 回复数