IAP flash write

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IAP flash write

2,100 次查看
ianbenton
Senior Contributor I

Just wondering about the sequence to write to the flash. . . 

I am going to write the area between 0xA000 and 0xFFFF, 512 bytes at a time (as in one block off a SD card).

First I prepared the whole area of flash for erase (CMD 50), erased it (CMD 51),

prepared it again (CMD 50) and then wrote to it (CMD 52).

After the first 512 bytes, it returns with error 9 (not prepared).

Does that mean that I should run the prepare command EACH time I run the write command?

Is the prepare command required for the erase operation?

标签 (2)
0 项奖励
回复
1 回复

1,940 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hello Ian,

I've checked the IAP Commands for both of the LPCs that were tagged on this post.To be extra sure of the information can you please provide the part number of the LPC you are using. 

However I believe the IAP commands are the same through out. You mention that you are erasing using CMD 51 and writing CMD 52. Can you please verify  these commands as they should be erase CMD 52 and write CMD 51. 

In addition, you should always prepare the sector prior an erase or write command. 

You can find more information in this application note.

Best Regards,

Sabina

0 项奖励
回复