I2C0 not work with lpcopn 1.03

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C0 not work with lpcopn 1.03

1,620 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by szantech on Sat Jul 13 09:08:12 MST 2013
Hi,
I have updated my lpcopen from 1.02 to 1.03. After updating I have adapted my code. All components work but I2C0 not. I have connected EEPROM on I2C0 and I2C1. I2C1 works fine but I2C0 not. It seems that the start condition is not detected and the application ends in an endless loop in Chip_I2C_EventHandlerPolling().
I'm using LPC4357. I have also attached the recorded signals.
Any idea?
Labels (1)
0 Kudos
Reply
1 Reply

1,594 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wellsk on Sat Jul 13 18:00:00 MST 2013
Look at this bug tracker issue related to the SCU mode definitions and incorrect pin states.
http://www.lpcware.com/content/bugtrackerissue/lpcopen-v103-scumodexxxx-and-mdxxx-names-and-comments...
0 Kudos
Reply