I2C in LPC824 with LPCOpen

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2C in LPC824 with LPCOpen

1,753件の閲覧回数
franciscopasten
Contributor I

Hi,

i need a simple example of the configuration of de i2c in LPC824.

It just need a continius connection, without using interruption or another routines.

thanks

0 件の賞賛
返信
1 返信

1,422件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I'd highly recommend you to refer to these I2C demo which are involved in the LPCOpen library.
LPCOpen library:
Have a great day,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信