I2C in LPC824 with LPCOpen

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C in LPC824 with LPCOpen

1,740 Views
franciscopasten
Contributor I

Hi,

i need a simple example of the configuration of de i2c in LPC824.

It just need a continius connection, without using interruption or another routines.

thanks

0 Kudos
Reply
1 Reply

1,409 Views
jeremyzhou
NXP Employee
NXP Employee
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I'd highly recommend you to refer to these I2C demo which are involved in the LPCOpen library.
LPCOpen library:
Have a great day,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply