I2C USER SPACE problem in uclnux on LPC1788 cortex m3 mio board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C USER SPACE problem in uclnux on LPC1788 cortex m3 mio board

906 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by shamvhgowda on Mon Feb 17 00:12:20 MST 2014
Hello Friends,

I am using Ububtu 12.04 version and doing uclinux on LPC 1788 Board.
Since I'm new to LPCware and also new to LPC1788 uclinux. I am writing Device drivers for LPC1788 uclinux . So i'm strucked in i2c communication protocol. So can anyone help me to solve this issue.

Here is my user space code

#include <signal.h>
#include <stdio.h>
#include <string.h>
#include <fcntl.h>
#include <linux/i2c.h>
#include <linux/i2c-dev.h>
#include <linux/kernel.h>

#include <linux/fs.h>


int main ( void )
{
int file;
int adapter_nr = 0; /* probably dynamically determined */
char filename[20];

char i = 0;
int  res;
char buf[8],Buffer1[8];
buf[0] = 00;     // Seconds
buf[1] = 00;   // Minutes
buf[2] = 00;      // Hours
buf[3] = 00;           // Day of week
buf[4] = 15;       // Date
buf[5] = 02;      // Month
buf[6] = 14;      // Year
buf[7] = 0x00;             // Control  = 00h
for(i=0; i<7; i++)
{
buf = RX8035_toBCD(buf);
}
//-- Set control bits
buf[2] &= 0x3F;    //-- Hours    bit 7(12/24) = 0(12-hour mode)
buf[5] &= 0x1F;



snprintf(filename, 19, "/dev/i2c-%d", adapter_nr);//Make sure to give mknod /dev/i2c-2 c 89 0 in target(minicom)
file = open(filename, O_RDWR);
if (file < 0)
{
printf("/* ERROR IN FILE OPEN\r\n");
return 0;
}
else
printf("File open Success\r\n");

int addr = 0x64; /* The I2C slave address(rtc) address */

if (ioctl(file, I2C_SLAVE, addr) < 0)
{
printf("/* ERROR IN ioctl \r\n");  
/* ERROR HANDLING; you can check errno to see what went wrong */
return 0;
}

/* Using I2C Write, equivalent of
i2c_smbus_write_word_data(file, register, 0x6543) */

if (write(file, buf, 8) != 8)
{
printf("/* ERROR IN write\r\n");
/* ERROR HANDLING: i2c transaction failed */

}
else
printf(" WRITE Succes %d\n",buf[0]);

int addr1 = 0x65; /* The I2C address */
if (ioctl(file, I2C_SLAVE_FORCE, addr1) < 0)
{
printf("/* ERROR IN ioctl \r\n");  
/* ERROR HANDLING; you can check errno to see what went wrong */
return 0;
}

/* Using I2C Read, equivalent of i2c_smbus_read_byte(file) */
if (read(file, Buffer1, 8) != 8)
{
printf("/* ERROR IN Read\r\n");
/* ERROR HANDLING: i2c transaction failed */
}
else
{
printf("Succes %d\n",Buffer1[0]);
/* buf[0] contains the read byte */
}


}

In target(minicom) i got error like this

~ # chmod +x i2capp
~ # ./i2capp
File open Success
/* ERROR IN writ------------[ cut here ]------------
WARNING: at kernel/irq/manage.c:274 0xa00865e7()
Unbalanced enable for IRQ 10
Modules linked in:
Backtrace: no frame pointer
---[ end trace 84d59ffaa05f0b6c ]---
e
/* ERROR IN Read
~ #

Any reply will be appreciated and i need reply soon because i am strucked from past 3 days. and tell me if i'm doing any thing wrong.

Thanq
Sham
Labels (1)
0 Kudos
Reply
0 Replies