I2C Example lpc1769 board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C Example lpc1769 board

4,768 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Alexander Gospodinov on Wed Apr 02 07:05:50 MST 2014
Hi,

i tried to run the periph_i2c example, which is included in the lpcopen_2_10_lpcxpresso_nxp_lpcxpresso_1769 data file. I am using the lpc1769 board, the base board and the lpcxpresso IDE, Debugging runs well but i don't get the main menu displayed on tera term. Has someone the same problem and can help me with this.

thank you in advance and best regards
Labels (1)
0 Kudos
Reply
10 Replies

4,659 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embeddedguy on Tue Apr 22 10:44:41 MST 2014
and another - direct reply to post rather than thread.
0 Kudos
Reply

4,659 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embeddedguy on Tue Apr 22 10:44:06 MST 2014
sorry - just testing a reply.
0 Kudos
Reply

4,659 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Alexander Gospodinov on Mon Apr 14 02:00:03 MST 2014
Hi,

i think i found the reason why the program doesn't run. I use the lpcopen_2_07_lpcxpresso_nxp_lpcxpresso_1769 release and this example runs well. Befor that i used release lpcopen_2_10_lpcxpresso_nxp_lpcxpresso_1769 and it doesn't run. So the error lies in the release software 2_10.
However now its running, but when i want do connect a device, should i connect this to the base board or to the lpc1769?

thanks and best regards
0 Kudos
Reply

4,659 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Alexander Gospodinov on Tue Apr 08 04:39:30 MST 2014
Jumper J7 are all connected. I have tried to run the periph_uart_rb and it runs well. And i can see the menu displayed in tera term. But when i run the periph_i2c it doesn't work. I also connected the pc to RxD and TxD signals, but i don't get a signal in tera term when starting the periph_i2c.
0 Kudos
Reply

4,659 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Mon Apr 07 18:58:01 MST 2014
Hi Alexander,
Check jumper J7 on baseboard. By default it All three should be connected. If it does not solve your problem, just probe RxD and TxD signals of FT232 as well as output signals DP and DM.
0 Kudos
Reply

4,659 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by atomicdog on Mon Apr 07 09:43:52 MST 2014
Have you tried a loop-back test to see if your com port is working?
Is the port setup for 8n1 and the correct baudrate?

The baseboard has a lot of jumpers. I would definitely double check the jumper settings.
0 Kudos
Reply

4,659 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Alexander Gospodinov on Mon Apr 07 07:45:45 MST 2014
Can it be possible, that i must set some Jumpers?
0 Kudos
Reply

4,659 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Alexander Gospodinov on Mon Apr 07 05:55:04 MST 2014
Hi,

i have already install FTDI drivers. I open the COM port which is connected to the X3 interface. I really don't know why this main menu isn't displayed. When i am debugging the program runs well and the main is showing "Running User Request".
0 Kudos
Reply

4,659 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Wed Apr 02 17:25:03 MST 2014
Hi Alexander,
Did you open correct COM port on your PC? You may also need to install FTDI drivers.
0 Kudos
Reply

4,659 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by atomicdog on Wed Apr 02 10:36:23 MST 2014
I just started playing with this example a few minutes ago. I see the menu display just fine. I'm not using the baseboard though. I connected straight to the TX3/RX3 pins.
0 Kudos
Reply