I would like to debug with LPC 824-max targeted using LPC-Link 2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I would like to debug with LPC 824-max targeted using LPC-Link 2

1,132 Views
kenishida
Contributor I

I would like to debug with LPC 824-max targeted using LPC-Link 2,

The following error appears.

02: Failed on connect   

Could not connect to core.  

 31: No connection to emulator device 

LPCXpresso RedlinkMulti Driver v 8.2 (Sep 5 2016 10: 12: 38 - crt _ emu _ cm _ redlink build 725) Failed on connect: Ee (36). Could not connect to core. No connection to emulator device 

Please tell me about the solution.

0 Kudos
Reply
1 Reply

1,060 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Ken Ishida,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
Please following these steps to solve this issue:
  1. Erase the flash of the LPC824;
  2. Update the firmware of the LPC-Link2, then try again.

Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply