I would like to debug with LPC 824-max targeted using LPC-Link 2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I would like to debug with LPC 824-max targeted using LPC-Link 2

1,141件の閲覧回数
kenishida
Contributor I

I would like to debug with LPC 824-max targeted using LPC-Link 2,

The following error appears.

02: Failed on connect   

Could not connect to core.  

 31: No connection to emulator device 

LPCXpresso RedlinkMulti Driver v 8.2 (Sep 5 2016 10: 12: 38 - crt _ emu _ cm _ redlink build 725) Failed on connect: Ee (36). Could not connect to core. No connection to emulator device 

Please tell me about the solution.

0 件の賞賛
返信
1 返信

1,069件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Ken Ishida,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
Please following these steps to solve this issue:
  1. Erase the flash of the LPC824;
  2. Update the firmware of the LPC-Link2, then try again.

Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信