I ask you about usage of lpc_dfuutil.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I ask you about usage of lpc_dfuutil.

1,091件の閲覧回数
hiromasashigema
Contributor II

How are you.

I have already used this community about 3 years ago concernibg to LPC1830.

I have used the libusb0 device driver from sourceforge for to communicate with LPC1830.

I want to change this driver to WinUSBNet or LibUsbDotNet for C#.

After the above change, is it necessay to give information to lpc_dfuutil.exe.

If you give me any comment, I am very happy.

 

Shiggy

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

925件の閲覧回数
graygirling
NXP Employee
NXP Employee

Hi

You should be able to find information about dfu-util from the maintainers at dfu-util Homepage.

There may be small differences between that version of dfu-util and the one distributed with LPCXpresso IDE, which might be older.

Some information is also provided using the command

dfu-util --help

Sincerely

LPCXpresso IDE Support

0 件の賞賛
返信