I/O configure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I/O configure

2,701 Views
lihai
Contributor II

LPC1788 when using ulink2 debug, all I/O output H level, can I configure to output Low level, and how to configure it.?

Labels (1)
Tags (1)
4 Replies

2,582 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Li Hai,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
The default configuration of GPIO is persevere, would make them output high level.
pastedImage_1.png
Have a great day,

TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,582 Views
lihai
Contributor II

Thank you, Mr jeremyzhou

Sorry I reply so late, thank you very much for your help. I know how to initial the Pin mode. But when I use keil4 download .hex file to Flash, all I/O output high level. Infact i need low level. so when download .hex file, can output low level?  

Have a great day!

0 Kudos
Reply

2,582 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Li Hai,

Thanks your reply.

I'm afraid that default setting of I/O is impossible to change.

Have a great day,

TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,582 Views
lihai
Contributor II

Hi jeremyzhou

    Thank you!In that case, I need redesigned my circuit. 

Have a great day.

0 Kudos
Reply