How to write CTS/RTS enabled UART application for LPCXpresso 18S37

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to write CTS/RTS enabled UART application for LPCXpresso 18S37

2,015件の閲覧回数
srikanthmediset
Contributor I

Hai,

    I am working on LPCXpresso 18S37 base board and I had run the sample UART application and I was succesful.Now I want to try UART application with CTS/RTS.So I want to know how to start it or if any sample application is available please share it.

Regards

srikanth

ラベル(1)
0 件の賞賛
返信
1 返信

1,846件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi, 

Unfortunately, there is no an example like you need, however you can check the following threads as reference. 

UART auto-flow control and doc error 

[SOLVED] LPC1778 hard fault during UART setup 

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信