How to use the LPC1114 board without the debugger board.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use the LPC1114 board without the debugger board.

2,164件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by zapta on Sat Aug 30 17:47:20 MST 2014
Hi all,

I got this board from Digikey http://www.digikey.com/product-detail/en/OM13014,598/568-7517-ND/2700004  and was able to build and run the examples on it (so far so good).

My next step is to separate between the debugger and the target board and use the target board in an actual design that exchange data with a computer via USB/Serial.

1. Where can I find the hardware manual of the above board?  Something that explain the various jumpers and headers and how to use the target half as a stand alone board.

2. If I separate the target board and run it independently connected to a USB port, where does it gets the 3.3V?  Can it regulate its own 3.3V from its USB +5V power?

3. I separate the target board and run it independently, is there a way to update its firmware from its USB port (via some bootloader) without having to connect the debugger board?

Thanks,

Z.

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,152件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by zapta on Tue Sep 02 15:27:28 MST 2014
Thanks.
0 件の賞賛
返信

2,152件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Tue Sep 02 13:08:02 MST 2014

Quote: zapta
Yes, I can read diagrams.



So what's not clear then?


Quote: zapta
Still no answer for #1, #2.



#1 Nowhere...

#2 You have to add your own 3.3V regulator  :((
0 件の賞賛
返信

2,152件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Tue Sep 02 13:08:00 MST 2014

Quote: zapta
Yes, I can read diagrams.



So what's not clear then?


Quote: zapta
Still no answer for #1, #2.



#1 Nowhere...

#2 You have to add your own 3.3V regulator  :((
0 件の賞賛
返信

2,152件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by zapta on Tue Sep 02 09:56:24 MST 2014
Thanks VingeshEP. Yes, I can read diagrams.

I found an answer for #3 in AN11305. Still no answer for #1, #2. My board is the LPC11U14 with a USB connector also on the target side. I could not find a manual for it, just schematic. Also, it doesn't seem to have a 3.3V regulator (from the USB +5V) so I can't see how the target board can work independently if separated from the debugger half.
0 件の賞賛
返信

2,152件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by VigneshEP on Tue Sep 02 05:13:07 MST 2014
http://www.lpcware.com/LPCXpressoV1Boards

Look for OM13014 for schematics. I hope you're able to read / understand circuit diagrams!

HTH!
0 件の賞賛
返信