How to use cockpit to get LMA by general card as type a or b w/ PN5180?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use cockpit to get LMA by general card as type a or b w/ PN5180?

1,859 Views
Frankfu1
Contributor I

Hi,

From AN11740 at page 50, I can see signals of LMA and AUX1. 

In my side, we already understood how to get AUX1 by cockpit. 

How to set the procedure for getting LMA by ISO1443-A or B?

My procedure it to set Reader\Load Protocol\Endless REQA\RF field on and use the pickup coil to get card information. Seems I ONLY can see RF field w/o tx waveform and LMA.

Plz guide us to get LMA.

Thanks,

Frankfu

Labels (1)
0 Kudos
Reply
4 Replies

1,837 Views
Frankfu1
Contributor I

Is it possible to sniffer LMA waveform w/ "general type A card" and pickup coil by cockpit and oscilloscope instead of AN12549?

As the video of ch3, https://www.nxp.com/video/nfc-antenna-design-4-optimization-debugging:ANTENNA-DEBUGGING-VIDEO

Or only ReferencePICC w/ AWG can see LMA waveform?

2021-08-23_155116.jpg

Thanks,

0 Kudos
Reply

1,832 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

This should also be possible. However, the accuracy should not be as good as AWG and reference PICC.

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 Kudos
Reply

1,823 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

I confirmed the question in the related team and recommend the customer uses the system of AN12549

0 Kudos
Reply

1,844 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Please refer to the Figure 6. Minimum test setup for LMA tests of the PN5190 antenna design guide as the link.
URL:https://www.nxp.com/docs/en/application-note/AN12549.pdf.
It is similar with PN5180.

Have a nice day.

 

Please refer to the Figure 6. Minimum test setup for LMA tests of the PN5190 antenna design guide as the link.
URL:https://www.nxp.com/docs/en/application-note/AN12549.pdf.
It is similar with PN5180.

0 Kudos
Reply