How to use Image authentication API ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use Image authentication API ?

1,854 Views
slou26
Contributor II

We need to check signature of an application located after the bootloader. We think use the image authentication api to do that. 

We tried to call  "skboot_authenticate" function without success ( HardFault ). Do you have an example for this ?

Tks

Regards,

Labels (1)
0 Kudos
Reply
1 Reply

1,783 Views
soledad
NXP Employee
NXP Employee

Hi,

Unfortunately, we don't have an example like you need, however you can check the following application notes:

https://www.nxp.com/docs/en/application-note/AN12283.pdf 

https://www.nxp.com/docs/en/application-note/AN12527.pdf 

Have a great day,
Sol

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply