How to use DAC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use DAC

2,050 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Frenchy on Mon Mar 14 04:28:17 MST 2016
Hello everyone,

I'm trying to use the DAC on my LPC4357 for a project and (if i understand the user manual well) I can configure the P4_4 pin as the output but i can't figure out where it is on the schematic...

If someone could help me, i'll be grateful.

(Sorry for my bad english  :bigsmile: , I hoped it was understandable)
标签 (1)
0 项奖励
回复
4 回复数

2,017 次查看
lpcware
NXP Employee
NXP Employee
bump
0 项奖励
回复

2,017 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Frenchy on Mon Mar 14 08:50:17 MST 2016
"In addition, the DAC output is shared with both,
ADC0 channel 0 (ADC0_0) and ADC1 channel 0 (ADC1_0)." page 384 in the user manual, i didn't pay enough attention, thanks for trying to help me.  ;-)

Edit : I see what you meant, i'm using the package LBGA256, i'm still not sure how tu use the dac, i'm trying to figure it out.
0 项奖励
回复

2,017 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Frenchy on Mon Mar 14 06:11:31 MST 2016
As i mentionned it, i'm using the LPC4357, i don't know if it's part of a special kind of board or smth...
0 项奖励
回复

2,017 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by starblue on Mon Mar 14 05:56:27 MST 2016
Which board are you using? Schematics doesn't make much sense for a naked controller. Which package? P4_4 is not available on TFBGA100 (see chapter "Pin configuration" of the user manual).
0 项奖励
回复