How to terminate running program?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to terminate running program?

2,366 Views
avswathi2892
Contributor I

Hi, 

I am new to mc programming. can i give a user input while the program is running and my program should take that input and act accordingly?

Thanks 

0 Kudos
Reply
2 Replies

2,304 Views
soledad
NXP Employee
NXP Employee

For the record, which device are you using?

Regards

0 Kudos
Reply

2,302 Views
soledad
NXP Employee
NXP Employee

Hi,

Yes, you can do it. Which IDE are you using?

Please check the document attached,  section 11 Debugging a Project.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply