How to setup LPC4370 HSADC via GPDMA with external signal triggering source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to setup LPC4370 HSADC via GPDMA with external signal triggering source

972件の閲覧回数
boonkongyip
Contributor I

Hi,

Has anybody has experience using LPC4370 HSADC via GPDMA with external signal as triggering source?

From the UM1053 user manual DMAMUX register, it seems to me that only SGPIO 14 or SGPIO 15 can act as triggering pin.

What is the setup require to trigger the GPDMA to start DMA from HSADC?

ラベル(2)
0 件の賞賛
返信
1 返信

832件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Boon Kong Yip,

To provide the fastest possible support I want to point you to refer to the LPC43xx CMSIS-Compliant standard peripheral firmware driver library which includes the GPDMA demo.

LPC43xx CMSIS-Compliant Standard Peripheral Firmware Driver Library (Keil, IAR) | www.LPCware.com 

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信