How to setup LPC4370 HSADC via GPDMA with external signal triggering source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to setup LPC4370 HSADC via GPDMA with external signal triggering source

1,373 Views
boonkongyip
Contributor I

Hi,

Has anybody has experience using LPC4370 HSADC via GPDMA with external signal as triggering source?

From the UM1053 user manual DMAMUX register, it seems to me that only SGPIO 14 or SGPIO 15 can act as triggering pin.

What is the setup require to trigger the GPDMA to start DMA from HSADC?

Labels (2)
0 Kudos
Reply
1 Reply

1,233 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Boon Kong Yip,

To provide the fastest possible support I want to point you to refer to the LPC43xx CMSIS-Compliant standard peripheral firmware driver library which includes the GPDMA demo.

LPC43xx CMSIS-Compliant Standard Peripheral Firmware Driver Library (Keil, IAR) | www.LPCware.com 

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply