How to save factory Firmware LPC55S69-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to save factory Firmware LPC55S69-EVK

4,518 Views
aryeduino
Contributor I

Hi All,

I am new to NXP boards and ARM Cortex 33.

I have just got my brand new  LPC55S69-EVK Board and I want to start developing and learn it more.
LPCxpresso55s69 Development Board:LPC55S69-EVK 

I have seen that there is a Firmware already install on it as an example from the factory - LED blinks and Audio in and out and also I have managed to get the Mouse doing a square with cursor as well.. These examples are neat and I want to keep (Specially the Audio) - How can I save the current Firmware on my LPC55S69-EVK Board?

Or maybe there is another way to enjoy the Firmware later on  after playing with the baord using the Example code and compile it and upload it.

As I have mentioned I am NEW and I am still learning - not trying so much now since I am not skilled as well as I do not want to loose the Firmware that is currently running.
I already downloaded the SDK for MCUXpresso IDE v11 - built it for Windows and it is already linked inside the IDE. (in the future I think to use Keil v5.5 as well with this board).

I hope that there is a way to preserve the Factory Firmware that it can be used and accessed in the future after erasing and flashing a new Firmware.

 

Thanks for your help

Aryeduino.

Labels (2)
0 Kudos
Reply
7 Replies

4,445 Views
al_bin
Contributor II

Getting Started with the LPC55S69-EVK Evaluation Board

says:

"OOB_test demo source code is available in SDK"

But I can't find it in:

mcuxpresso.nxp.com/en/builder?hw=LPCXpresso55S69

or any other places.

It is realy avaliable?

 

0 Kudos
Reply

4,431 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello al_bin,

I haven't find the OOB_test demo under SDK, while it seems you can have a look at the SDK demo "lpcxpresso55s69_multi_peripherals_test".

 

BR

Alice

4,428 Views
al_bin
Contributor II

Thank you. This is it.

Albert

0 Kudos
Reply

4,491 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello aryeduino,

This is J-link command function, no related with mcu, you can use read memory command :

 

Mem32

Read memory from the target system in units of 32-bits. If necessary, the target CPU is halted in order to read memory.

Syntax

Mem32 [<Zone>:]<Addr>, <NumItems> (hex)

Parameter Meaning
Zone Name of memory zone to access.
Addr Start address.
NumItems Number of items to read. Maximum is 0x100000.

Example

Mem32 0x0, 100 

 

About detail you can have a look at: 

https://wiki.segger.com/J-Link_Commander#Mem32   

 

BR

Alice

0 Kudos
Reply

4,499 Views
aryeduino
Contributor I

Thanks @Alice_Yang 

As I have mentioned I am new to NXP programing and I am familiar with STM32 a bit - I normally work with ESP and Arduino and I want to start learning NXP boards and ARM Cortex M33 for IoT Security as well.

I am not sure I fully understand what you suggest me to do. And I would be happy if you elaborate a bit an the steps needed to be taken in order to back it up.

Thanks

0 Kudos
Reply

4,509 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello aryeduino,

You can try to use J-link commander read all the flash data out, save it, next time you can grogram it to use. Or enter ISP mode (Detail refer to UM) using buttons on board, then using Blhost read the data out to a file .

Alice_Yang_0-1640223039801.png

 

BTW, as beginner, recommend use SDK demo:  

https://mcuxpresso.nxp.com/en/select  

 

 BR

Alice

0 Kudos
Reply

4,498 Views
aryeduino
Contributor I

Thanks @Alice_Yang 

As I have mentioned I am new to NXP programing and I am familiar with STM32 a bit - I normally work with ESP and Arduino and I want to start learning NXP boards and ARM Cortex M33 for IoT Security as well.

I am not sure I fully understand what you suggest me to do. And I would be happy if you elaborate a bit an the steps needed to be taken in order to back it up.

I have already downloaded and installed the SDK for board LPC55S69-EVK in my MCUXpresso - If there is a way to get the factory Firmware back from there I would be happy to know as well.

Thanks

0 Kudos
Reply