How to run code in SDRAM of LPC4088 ? Please Help!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to run code in SDRAM of LPC4088 ? Please Help!

923 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by agoodman on Sun Oct 26 07:12:54 MST 2014
My code is downloaded to on-chip flash with MDK4.72 .
This is my process:
1.initialize SDRAM
2.Copy code to SDRAM
3.configurate MPU
4.change PC with an function

However,PC won't change and CPU won't go to SDRAM to run codes.
Here are the codes:

void copy_to_SDRAM(void)                  
{
        void (*call_app)(void) = (void (*)(void))0xA00002CC;                   // pointer to user codes

memcpy((void *)0xA0000000,(void *)0x00000000,0x0007FFFF);    //copy (512K) on-chip flash's codes to SDRAM

__set_MSP(0xA00002C8);

call_app();             //jump to SDRAM to run
}

/*********************************************MPU setting *********************************************************/
/* Region size definitions */

#define MPU_REGION_SIZE_32KB    0x0E
#define MPU_REGION_SIZE_64KB    0x0F
#define MPU_REGION_SIZE_512KB   0x12
#define MPU_REGION_SIZE_32MB    0x18
#define MPU_REGION_SIZE_128MB   0x1A

#define MPU_REGION_SIZE_1GB     0x1D
#define MPU_REGION_SIZE_2GB     0x1E
#define MPU_REGION_SIZE_4GB     0x1F

/* Access permission definitions */
#define MPU_FULL_ACCESS                         0x03

/* RASR bit definitions */
#define MPU_RASR_REGION_SIZE(n)         ((uint32_t)(n<<1))
#define MPU_RASR_ACCESS_PERMISSION(n)   ((uint32_t)(n<<24))
#define MPU_REGION_ENABLE               ((uint32_t)(1<<0))

void board_mpu_init(void)
{
  MPU->CTRL = 0x00;
  __ISB();

    /* - Region 0: 0x00000000 - 0x0007FFFF --- on-chip non-volatile memory
     *      + Size: 512kB
     *      + Acess permission: full access
     */
    MPU->RNR  = 0;//indicate MPU region 0 
    MPU->RBAR = 0x00000000; // update the base address for the region 0
    MPU->RASR = MPU_RASR_ACCESS_PERMISSION(MPU_FULL_ACCESS)     //full access
                |MPU_RASR_REGION_SIZE(MPU_REGION_SIZE_512KB)    //512Kb size
                |MPU_REGION_ENABLE;                             //region enable

    /* - Region 1: 0x10000000 - 0x1000FFFF --- on-chip SRAM
     *      + Size: 64kB
     *      + Access permission: full access
     */
    MPU->RNR = 1;
    MPU->RBAR = 0x10000000; // update the base address for the region 1
    MPU->RASR = MPU_RASR_ACCESS_PERMISSION(MPU_FULL_ACCESS)
                |MPU_RASR_REGION_SIZE(MPU_REGION_SIZE_64KB)
                |MPU_REGION_ENABLE;

     /* - Region 2: 0x40000000 - 0x400FFFFF --- APB peripheral
     *      + Size: 1MB
     *      + Access permission: full access
     */
    MPU->RNR = 2;
    MPU->RBAR = 0x40000000; // update the base address for the region 2
    MPU->RASR = MPU_RASR_ACCESS_PERMISSION(MPU_FULL_ACCESS)
                |MPU_RASR_REGION_SIZE(MPU_REGION_SIZE_1MB)
                |MPU_REGION_ENABLE;

     /* - Region 3: 0x20080000 - 0x200BFFFF --- AHB peripheral
     *      + Size: 256KB
     *      + AP=b011: full access
     */
    MPU->RNR = 3;
    MPU->RBAR = 0x20080000; // update the base address for the region 3
    MPU->RASR = MPU_RASR_ACCESS_PERMISSION(MPU_FULL_ACCESS)
                |MPU_RASR_REGION_SIZE(MPU_REGION_SIZE_256KB)
                |MPU_REGION_ENABLE;

     /* - Region 4: 0xE0000000 - 0xE00FFFFF --- System control
     *      + Size: 1MB
     *      + Access permission: full access
     */
    MPU->RNR = 4;
    MPU->RBAR = 0xE0000000; // update the base address for the region 4
    MPU->RASR = MPU_RASR_ACCESS_PERMISSION(MPU_FULL_ACCESS)
                |MPU_RASR_REGION_SIZE(MPU_REGION_SIZE_1MB)
                |MPU_REGION_ENABLE;

     /* - Region 5:0x20000000 - 0x20007FFF --- on chip SRAM
     *      + Size: 32kB
     *      + Access permission: full access
     */
    MPU->RNR = 5;
    MPU->RBAR = 0x20000000; // update the base address for the region 5
    MPU->RASR = MPU_RASR_ACCESS_PERMISSION(MPU_FULL_ACCESS)
                |MPU_RASR_REGION_SIZE(MPU_REGION_SIZE_32KB)
                |MPU_REGION_ENABLE;

    /* - Region 6:0x80000000 - 0x87FFFFFF --- NandFlash
    *      + Size: 128MB
    *      + Access permission: full access
    */
   MPU->RNR = 6;
   MPU->RBAR = 0x80000000; // update the base address for the region 5
   MPU->RASR = MPU_RASR_ACCESS_PERMISSION(MPU_FULL_ACCESS)
               |MPU_RASR_REGION_SIZE(MPU_REGION_SIZE_128MB)
               |MPU_REGION_ENABLE;

    /* - Region 7:0xA0000000 - 0xA1FFFFFF --- Ext SDRAM
    *      + Size: 32MB
    *      + Access permission: full access
    */
   MPU->RNR = 7;
   MPU->RBAR = 0xA0000000; // update the base address for the region 5
   MPU->RASR = MPU_RASR_ACCESS_PERMISSION(MPU_FULL_ACCESS)
               |MPU_RASR_REGION_SIZE(MPU_REGION_SIZE_32MB)
               |MPU_REGION_ENABLE;

   MPU->CTRL =(1<<0);      //Enable the MPU
   __DSB();
   __ISB();

}


Labels (1)
0 Kudos
Reply
0 Replies