How to regain debug access if SWDIO and SWDCLK are both disabled via the switch matrix.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to regain debug access if SWDIO and SWDCLK are both disabled via the switch matrix.

2,271件の閲覧回数
donaldngai
Contributor I

While familiarising myself with the LPC812, I disabled all the fixed functions via the switch matrix. As a result, my LPC812 can't be connected to with LPCXpresso. I tried to enter into ISP mode using the instructions here: https://community.nxp.com/thread/389040 . But that does not seem to work. I hypothesize that it's partly because of both SWDIO and SWDCLK both being disabled. Is there anyway to reset the switch matrix to regain debug access? 

Thanks!

0 件の賞賛
返信
2 返答(返信)

2,055件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

The ISP reset over debug function will only help if your board has the appropriate signal wired between the chip and debug connector. Try booting into ISP mode yourself by pulling the ISP to ground as you power your board up, as detailed in Regaining debug access to target MCU 

[You'll need to do this for using Flash Magic, as well as for trying to regain debug access.]

Regards,

LPCXpresso Support

0 件の賞賛
返信

2,055件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Could you please try using FlashMagic tool?

Flash Magic - Supported Devices 

I hope this helps.


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信