How to recognise LPC4088 as a USB device?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to recognise LPC4088 as a USB device?

跳至解决方案
1,724 次查看
avinashh
Contributor III

Hi,

I have used USB device interface of LPC4088 processor in our application.

Now am not getting how to test this as a device with windows PC.

How to recognize LPC4088 as a USB device? Is there any driver for LPC4088 for windows?

regards,

Avinash

标签 (2)
标记 (1)
0 项奖励
回复
1 解答
1,410 次查看
avinashh
Contributor III

Hi soledad,

Thanks for your reply.

The issue got resolved.

The problem was USB clock. We varied the clock speed and the problem got resolved.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,411 次查看
avinashh
Contributor III

Hi soledad,

Thanks for your reply.

The issue got resolved.

The problem was USB clock. We varied the clock speed and the problem got resolved.

0 项奖励
回复
1,410 次查看
avinashh
Contributor III

I'm able to see the device as Unkown Device.

Can anyone suggest how to start communication with the host?

0 项奖励
回复
1,410 次查看
soledad
NXP Employee
NXP Employee

Hello,

You can download LPCXpresso from the next link:

LPCXpresso IDE v8.2.2|NXP 

After download and install it you can find some LPCOpen examples for the LPC4088 device. In these examples are included USB examples that you can debug and use.

In addition please check the below link:

USB with NXP Microcontrollers | www.LPCware.com 

Please let me know if this helps!!

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复