How to load bootloader into external SPI flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to load bootloader into external SPI flash

2,307件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sudhir_reddy83 on Tue Jul 10 22:03:06 MST 2012
Hi,



I am developing a prototype using LPC4330FBD144.
I am newbie to LPC4330 but I already worked with LPC1788.
I am using M25P40 SPI flash device to store the bootloader program for LPC4330.

1. I want to know what are the ways in which I can download the bootloader into external SPI flash device.
2. I also want to know if there is any way to download the bootloader using ISP into external SPI flash device.


Please do help me in this regard.


Thank You in Advance
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,171件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by a5856 on Wed Aug 08 06:31:13 MST 2012
For my device PM25LV010 I modified programming algorithm for DFUsec utility.
Note, that chip on HItex board and M25P40 are using different command set and connection to LPC4300.
For booting from M25P40 you can use SPI(SSP) interface.
0 件の賞賛
返信

2,171件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by PhilYoung on Tue Aug 07 14:40:04 MST 2012
you can do this with flash magic, you may need to provide the programmer code for it to download, but there are examples included with it for the Hitex board which might work, or at least be a good starting point.
0 件の賞賛
返信

2,171件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by research on Mon Aug 06 22:00:10 MST 2012
Hi,

we are using LPC1788FBD144. can you help me to write a ethernet bootloader.  I am getting problem in Init PLL.  if your are using , can you send me the procedure.

Thanks & Advance
Sivakami
0 件の賞賛
返信