How to handle the linking error L6971E

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to handle the linking error L6971E

4,643件の閲覧回数
elviswang
Contributor I


Hi,

 

I am using the LPC 1788, and after adding an usb host lite project to an existing project, I have met the linking error with all files compiling right.

 

".\Flash\LPC1788_OMR.axf: Error: L6971E: s_single_read.o(.data) type RW incompatible with main_program.o(.ARM.__AT_0x10003650) type ZI in er RW_IRAM1. "

 

The following figure is the R/W Memory set. And also I has attached the .map file.

 

And I am seeking help for what is the reason of this error and how to handle this kind of error?

 

Many thanks.

 

155389_155389.pngpastedImage_0.png

Original Attachment has been moved to: LPC1788_OMR.map.zip

ラベル(3)
タグ(2)
0 件の賞賛
返信
1 返信

3,600件の閲覧回数
rolfmeeser
NXP Employee
NXP Employee

It is probably better to ask this on the Keil/ARM website.

From my limited knowledge of the issue it appears your extensive use of absolute variable placements somehow creates this conflict of section attributes (RW vs. ZI), but I may be wrong...

0 件の賞賛
返信