How to get start with emwin library for LPC2478 ?. Where can I download BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to get start with emwin library for LPC2478 ?. Where can I download BSP

2,221件の閲覧回数
supuntharanga
Contributor I

Hi,

I'm new to embedded UI. I want to know how to use emwin library to create GUI. I searched over internet and found that it needs to download a BSP. Is there any similar BSP which can be used with LPC2478 ?.

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,978件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

If you are developing a new project based on the LPC24xx, please consider that it is part of the legacy devices, and resources/compatibility may be limited. For LCD/GUIs support, you may consider the newer LPC54xxx family, with integrated Flash and RAM.

 

Regarding emWin features, you could refer to the documentation/User Guide:   https://www.nxp.com/pages/emwin-graphics-library:EMWIN-GRAPHICS-LIBRARY?tab=Documentation_Tab

In case of having specific emWin issues/questions, you could directly contact Segger:

https://www.segger.com/products/user-interface/emwin/


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,978件の閲覧回数
rle
Contributor I

I currently have emwin version 5.16d. Where can I download the latest version (5.48 perhaps). Thank you.

0 件の賞賛
返信