How to get SPI Example Working with SPI1 as Master?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to get SPI Example Working with SPI1 as Master?

2,310件の閲覧回数
mazarfarran
Contributor I

Hello,

I'm trying to get the SPI example project "periph_spi_sm_int" working with SPI1 as the master and SPI0 as the slave.  The example worked when SPI0 was the master, but switching the two gives this output:

SLAVE [txDoneCount = 1, rxDoneCount = 0]
MASTER [txDoneCount = 16, rxDoneCount = 16]

TRANSFER COMPLETE: errors = 0
Master total transfer time = 18893uS
Showing data from : Master TX data
0x0121 0x0122 0x0123 0x0124 0x0125 0x0126 0x0127 0x0128
0x0129 0x012a 0x012b 0x012c 0x012d 0x012e 0x012f 0x0130
Showing data from : Master RX data
0xffff 0xffff 0xffff 0xffff 0xffff 0xffff 0xffff 0xffff
0xffff 0xffff 0xffff 0xffff 0xffff 0xffff 0xffff 0xffff
Showing data from : Slave TX data
0xfede 0xfedd 0xfedc 0xfedb 0xfeda 0xfed9 0xfed8 0xfed7
0xfed6 0xfed5 0xfed4 0xfed3 0xfed2 0xfed1 0xfed0 0xfecf
Showing data from : Slave RX data
0x0000 0x0000 0x0000 0x0000 0x0000 0x0000 0x0000 0x0000
0x0000 0x0000 0x0000 0x0000 0x0000 0x0000 0x0000 0x0000

I have tried switching the MOSI and MISO pins, but got the same result.  The only change I made to the example was switching the macros:

/* Board specific example setup */
//#define SPIMASTERIRQHANDLER                 SPI0_IRQHandler
//#define LPC_SPIMASTERPORT                   LPC_SPI0
//#define LPC_SPIMASTERIRQNUM                 SPI0_IRQn
//#define SPISLAVEIRQHANDLER                  SPI1_IRQHandler
//#define LPC_SPISLAVEPORT                    LPC_SPI1
//#define LPC_SPISLAVEIRQNUM                  SPI1_IRQn

#define SPIMASTERIRQHANDLER                 SPI1_IRQHandler
#define LPC_SPIMASTERPORT                   LPC_SPI1
#define LPC_SPIMASTERIRQNUM                 SPI1_IRQn
#define SPISLAVEIRQHANDLER                  SPI0_IRQHandler
#define LPC_SPISLAVEPORT                    LPC_SPI0
#define LPC_SPISLAVEIRQNUM                  SPI0_IRQn

Thanks

タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,043件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Mazar Farran,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.

Before answer this question, I was wondering if you can tell me which chip you use.

I'm looking forward to your reply.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,043件の閲覧回数
mazarfarran
Contributor I

Hi Ping,

I'm using the LPC54102J512 chip.  The board is the LPCXpresso54102.

Thank you!

Mazar

0 件の賞賛
返信