How to enable function SGPIO to meet SFF-8485 Specification SFF-8485 REV0.7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable function SGPIO to meet SFF-8485 Specification SFF-8485 REV0.7

Jump to solution
8,791 Views
carter_wang
Contributor I

 

Hi,

 

We use chip LPC5526JBD64E to get the status of hard drives from the host via SGPIO.

I was wondering whether the chip supports the SGPIO function?
If the answer is yes, how to enable it?

 

BR,

carter

0 Kudos
Reply
1 Solution
8,746 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Cater

Here are some  application notes on how to use SGPIO on LPC4300. If source codes exist, they are included in the zip files:

SGPIO on the LPC4300:
https://www.nxp.com/docs/en/application-note/AN11275.zip

Using SGPIO to emulate an SPI master interface:
https://www.nxp.com/docs/en/application-note/AN11210.zip

LPC4300 camera interface design using SGPIO:
https://www.nxp.com/docs/en/application-note/AN11196.zip

SGPIO camera module design using LPC4300:
https://www.nxp.com/docs/en/application-note/AN11343.zip

Implementing a UART using SGPIO on LPC4300:
https://www.nxp.com/docs/en/application-note/AN11351.zip

 

Hope this helps.

Jun Zhang

View solution in original post

0 Kudos
Reply
7 Replies
8,774 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Carter

Please read this application note. this is 

https://www.nxp.com.cn/docs/en/application-note/AN12326.pdf

but we don't have qualification of SFF-8485 Specification. 

Have a nice day,

Jun Zhang

0 Kudos
Reply
8,770 Views
carter_wang
Contributor I

 

Hi Jun,

 

Thanks for your information.

However, I am looking forward to Serial General Purpose Input Output(SGPIO), not secure gpio.

 

BR,

carter

0 Kudos
Reply
8,762 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Cater.

No. LPC55 doesn't support Serial General Purpose Input Output(SGPIO).

our LPC43xx supports Serial GPIO, but LPC55 doesn't.

Hope this helps,

Jun Zhang

0 Kudos
Reply
8,757 Views
carter_wang
Contributor I

 

Hi Jun,

 

Got it.

I was wondering if you could share the source code of SGPIO with us?

 

BR,

carter

0 Kudos
Reply
8,747 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Cater

Here are some  application notes on how to use SGPIO on LPC4300. If source codes exist, they are included in the zip files:

SGPIO on the LPC4300:
https://www.nxp.com/docs/en/application-note/AN11275.zip

Using SGPIO to emulate an SPI master interface:
https://www.nxp.com/docs/en/application-note/AN11210.zip

LPC4300 camera interface design using SGPIO:
https://www.nxp.com/docs/en/application-note/AN11196.zip

SGPIO camera module design using LPC4300:
https://www.nxp.com/docs/en/application-note/AN11343.zip

Implementing a UART using SGPIO on LPC4300:
https://www.nxp.com/docs/en/application-note/AN11351.zip

 

Hope this helps.

Jun Zhang

0 Kudos
Reply
8,620 Views
carter_wang
Contributor I

 

Hi Jun,

 

I tried to simulate SGPIO slave device via sensing gpio signals by software.

However, it seems impossible.

Am I right?

 

BR,

carter

0 Kudos
Reply
8,721 Views
carter_wang
Contributor I

 

Hi Jun,

 

Thanks for your information.

Have a good day~

 

BR,

carter

0 Kudos
Reply