How to download NXBUSBlib source code for LPC435X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to download NXBUSBlib source code for LPC435X

2,846 Views
ssudhir
Contributor II

We use LPC435X processor and would like to use the USB ROM stack and use NXBUSBlib. We used

www.lpcware.com/content/project.nxpUSBlib to download the source code and couldn’t find there. Where I we find source code for NXBUSBLib and also manual for using USB ROM stack?

Thanks

Tags (1)
0 Kudos
Reply
5 Replies

2,710 Views
ssudhir
Contributor II

LlPC435X still support USB ROM Stack for HID or communication class?

0 Kudos
Reply

2,710 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

There is USBD Library for LPC4300/LPC1800 series MCUs

https://www.nxp.com/docs/en/application-note/TN00041.zip 

Please check if this can help you.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,710 Views
ssudhir
Contributor II

Thank Jun Zhang.

As we mentioned, we are using LPC4357 and want to use one UBS controller as a host and communicate using Mass Storage class and  another one in device mode and use either HID or communication (want to connect to a window host and window host can send configuration info to our board through this port). Do have any vendor suggestions  which support dual mode USB driver ?  Since we want to use one controller as host and another one as device we are guessing OTG mode won't work for us.

Thanks

0 Kudos
Reply

2,710 Views
bernhardfink
NXP Employee
NXP Employee

Thesycon is a very good provider of USB stacks for the LPC1800 and LP4300:

Website Thesycon

Regards,

Bernhard.

0 Kudos
Reply

2,710 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi SS,

I was informed we stopped maintaining lpcusblib and there is no support provided.

If user needs usb demo code, please use lpcopen which can be downloaded from this url

LPCOpen Software for LPC43XX | NXP 

Thanks for your understanding.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply