How to create a 1us Timer16_1_IRQHandler

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to create a 1us Timer16_1_IRQHandler

1,189 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ethan_kao on Mon Feb 02 23:57:26 MST 2015
Dear all,

    For my application in LPC1113, need a 1us unit timer to count, below is my timer definition
    I also use one I/O output to measure the cycle time of TIMER16_1_IRQHandler function
    I measure the I/O from LOW to HIGH is 1.76us; I/O from HIGH to LOW is 1.62us
    Is it means my code need more than 1us execute time?  :((
    Is 1us timer is possible or I miss something??

void main
{
    init ...
    init_timer16(1, 48M/1M );
    init ...
    timerResetflag1=0;
}

void init_timer16(uint8_t timer_num, uint32_t TimerInterval)
{
  if ( timer_num == 1 )
  {
    /* Some of the I/O pins need to be clearfully planned if
    you use below module because JTAG and TIMER CAP/MAT pins are muxed. */
    LPC_SYSCON->SYSAHBCLKCTRL |= (1<<8);
    LPC_IOCON->PIO1_10          &= ~0x07;
    LPC_IOCON->PIO1_10          |= 0x02;/* Timer1_16 MAT1 */

    LPC_TMR16B1->MR0 = TimerInterval;
    LPC_TMR16B1->MCR = 3;/* Interrupt and Reset on MR0 */

    /* Enable the TIMER1 Interrupt */
    NVIC_EnableIRQ(TIMER_16_1_IRQn);
  }
  return;
}

void TIMER16_1_IRQHandler(void)
{
        //GPIOSetValue(1,2,0);
LPC_TMR16B1->IR = 1;// clear interrupt flag
timer16_1_counter++;
 
if(timerResetflag1==1)//when re-enable timer, reset counter
{
timer16_1_counter=0;
timerResetflag=0;
timerResetflag1=0;
}
        //GPIOSetValue(1,2,1);
return;
}
标签 (1)
0 项奖励
回复
1 回复

1,150 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Thu May 07 20:24:52 MST 2015
Hi cortex-m0 has 16 clock cycle of interrupt latency with 0 wait state memory. A 1us timer interrupt is not possible:(.
0 项奖励
回复