Hi @lb_h
There is no direct tool available to convert MCUXpresso projects to Keil projects. However, you can manually import the source code and configuration files from the MCUXpresso project into a new Keil project. Here are the general steps to follow:
Create a new Keil project with the same target microcontroller as your MCUXpresso project.
Add the necessary header files, source files, and configuration files from your MCUXpresso project to the Keil project.
Update the include paths and defines in the Keil project to match those used in the MCUXpresso project.
Configure the Keil project settings, such as compiler options, linker options, and debugger settings, to match those used in the MCUXpresso project.
Build and debug the Keil project to ensure that it works correctly.
BR
Hang