How to change the xtal frequency slightly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to change the xtal frequency slightly

1,243 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ivar on Mon Jul 14 20:32:21 MST 2014
Is there any way to change the xtal frequency slightly so that i can achive the desired working frequency.

My board with LPC1830 has a 12 Mhz xtal. The processor run with 120 MHz.

I want to change the frequency at about 20 kHz to minimize RF interference in another circuit. Is it possible to make this adjustment?

Thank you.

Ivar.
Labels (1)
0 Kudos
Reply
2 Replies

1,226 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ivar on Fri Jul 18 12:18:56 MST 2014
Ok, I'll try that.

Thank you very much.

Ivar
0 Kudos
Reply

1,226 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Fri Jul 18 10:23:25 MST 2014
Hi,

Changing the load capacitance on the crystal pins, may shift the frequency by a few percent. There will not be any drastic changes in frequency though.

Thanks
NXP Technical Support
0 Kudos
Reply