How to cancell using PLL1 lock sequence.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to cancell using PLL1 lock sequence.

1,608件の閲覧回数
iwaomizota
Contributor I

Hi all,

I use LPC4357.

I would like to make a sequnce to use IRC as BASE_M4_CLK source until wating PLL 1 to lock.

There are 9 STEP  on c hpater 13.2.2.1 of "UM10503".

4.Reconfigure PLL1 as fllows.

5.Wait for the PLL1 to lock.

Could you please tell me how to cancel using crystal oscillator as clock source for PLL1 and go back to use IRC before PLL 1 is locked on STEP5?

Best Regards.

ラベル(1)
0 件の賞賛
返信
1 返信

1,414件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Iwao Mizota,

    PLL1 source can be changed in register PLL_CTRL[CLK_SEL]. If you want to use the IRC, please set the CLK_SEL =0X01 instead of 0x06.

    pastedImage_1.png

Wish it helps you!

If you still have question, please contact me!


Have a great day,

Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信