How to calculate CAN BAUD RATE for lpc2129.....?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to calculate CAN BAUD RATE for lpc2129.....?

1,987件の閲覧回数
akhileshverneka
Contributor II

How to calculate CAN BAUD RATE for LPC2129....?

0 件の賞賛
返信
1 返信

1,909件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Akhilesh Vernekar

Please have a look at the Table 262. Bus Timing Register (BTR: CAN1BTR - address 0xE004 4014, CAN2BTR -
address 0xE004 8014, CAN3BTR - address 0xE004 C014, CAN4BTR - address
0xE005 0014) bit description  for TSEG2 field as attached.

can_baudrate_equation.png

In summary, the equation is simple as  VPB/(BRP+1)/(TESG1+TSEG2+3).

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信