How to allocate heap memory to external SDRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to allocate heap memory to external SDRAM

4,541 次查看
nithin3200
Contributor IV

Hi,

Am using LPC546xx series microcontroller on  custom-made board, emwin is used for GUI and my ide is MCUXpresso only. When am using internal memory emwin is working fine. After that  memory is increased so am trying to allocate heap memory to external SDRAM(W9825G6KH-6I).Unfortunately that moment emwin is not working.

So any one can suggest me how to allocate heap memory to external SDRAM?.

标签 (3)
0 项奖励
回复
5 回复数

4,514 次查看
nithin3200
Contributor IV

Hi @Alice_Yang ,

Thanks for your replay.

As per your suggestion I made simple project to test SDRAM. So far am not using the debugger in our project and am using the uart for
verifying the program flow .

After checking the SDRAM test code  am getting error that Data buss success, address bus failure and last bit of data get corrupted.

-----------------------------------------------------Please find the below code for your reference------------------------------------------------------

status_t SDRAM_DataBusCheck(volatile uint32_t *address)
{
uint32_t data = 0;

/* Write the walking 1's data test. */
for (data = 1; data != 0; data <<= 1)
{
*address = data;

/* Read the data out of the address and check. */
if (*address != data)
{
return kStatus_Fail;
}
}
return kStatus_Success;
}

status_t SDRAM_AddressBusCheck(volatile uint32_t *address, uint32_t bytes)
{
char xyz[10];
uint32_t pattern = 0x55555555;
uint32_t size = bytes / 4;
uint32_t offset;
uint32_t checkOffset;

/* write the pattern to the power-of-two address. */
for (offset = 1; offset < size; offset <<= 1)
{
address[offset] = pattern;
}
address[0] = ~pattern;

/* Read and check. */
for (offset = 1; offset < size; offset <<= 1)
{
if (address[offset] != pattern)
{
sprintf(xyz,"%x",address[offset]);
USART_WriteByte(NIBP_USART,xyz[0]);
USART_WriteByte(NIBP_USART,xyz[1]);
USART_WriteByte(NIBP_USART,xyz[2]);
USART_WriteByte(NIBP_USART,xyz[3]);
USART_WriteByte(NIBP_USART,xyz[4]);
USART_WriteByte(NIBP_USART,xyz[5]);
USART_WriteByte(NIBP_USART,xyz[6]);
USART_WriteByte(NIBP_USART,xyz[7]);
USART_WriteByte(NIBP_USART,'-');

return kStatus_Fail;
}
}

if (address[0] != ~pattern)
{
USART_WriteByte(NIBP_USART,'W');
return kStatus_Fail;
}

/* Change the data to the revert one address each time
* and check there is no effect to other address. */
for (offset = 1; offset < size; offset <<= 1)
{
address[offset] = ~pattern;
for (checkOffset = 1; checkOffset < size; checkOffset <<= 1)
{
if ((checkOffset != offset) && (address[checkOffset] != pattern))
{

 

return kStatus_Fail;
}
}
address[offset] = pattern;
}
return kStatus_Success;
}
void BOARD_TestSDRAM(void)
{
char xyz[10];
uint32_t *sdram = (uint32_t *)SDRAM_BASE_ADDR;
uint8_t index;

if (SDRAM_DataBusCheck(sdram) != kStatus_Success)
{
USART_WriteByte(NIBP_USART,'D');
USART_WriteByte(NIBP_USART,'B');
USART_WriteByte(NIBP_USART,'F');
USART_WriteByte(NIBP_USART,'-');

// PRINTF("\r\n SDRAM data bus check is failure.\r\n");
}
else if (SDRAM_DataBusCheck(sdram) == kStatus_Success)
{
USART_WriteByte(NIBP_USART,'D');
USART_WriteByte(NIBP_USART,'B');
USART_WriteByte(NIBP_USART,'S');
USART_WriteByte(NIBP_USART,'-');

}
if (SDRAM_AddressBusCheck(sdram, SDRAM_SIZE_BYTES) != kStatus_Success)
{
USART_WriteByte(NIBP_USART,'A');
USART_WriteByte(NIBP_USART,'B');
USART_WriteByte(NIBP_USART,'F');
USART_WriteByte(NIBP_USART,'-');

// PRINTF("\r\n SDRAM address bus check is failure.\r\n");
}
else if (SDRAM_AddressBusCheck(sdram, SDRAM_SIZE_BYTES) == kStatus_Success)
{
USART_WriteByte(NIBP_USART,'A');
USART_WriteByte(NIBP_USART,'B');
USART_WriteByte(NIBP_USART,'S');
USART_WriteByte(NIBP_USART,'-');

}

USART_WriteByte(NIBP_USART,'D');
USART_WriteByte(NIBP_USART,'S');
USART_WriteByte(NIBP_USART,'W');

// PRINTF("\r\n Start EMC SDRAM access example.\r\n");
// PRINTF("\r\n SDRAM Write Start, Start Address 0x%x, Data Length %d !\r\n", sdram, SDRAM_EXAMPLE_DATALEN);

for (index = 0; index < SDRAM_EXAMPLE_DATALEN; index++)
{
*(uint32_t *)(sdram + index) = index;
}

// PRINTF("\r\n SDRAM Write finished!\r\n");

// PRINTF("\r\n SDRAM Read/Check Start, Start Address 0x%x, Data Length %d !\r\n", sdram, SDRAM_EXAMPLE_DATALEN);

for (index = 0; index < SDRAM_EXAMPLE_DATALEN; index++)
{
if (*(uint32_t *)(sdram + index) != index)
{
USART_WriteByte(NIBP_USART,'E');
USART_WriteByte(NIBP_USART,'R');
USART_WriteByte(NIBP_USART,'R');
USART_WriteByte(NIBP_USART,'-');
sprintf(xyz,"%x",index);
USART_WriteByte(NIBP_USART,xyz[0]);
USART_WriteByte(NIBP_USART,xyz[1]);
// PRINTF("\r\n SDRAM Write Data and Read Data Check Error!\r\n");
break;
}
}
USART_WriteByte(NIBP_USART,'D');
USART_WriteByte(NIBP_USART,'O');
USART_WriteByte(NIBP_USART,'N');
USART_WriteByte(NIBP_USART,'E');
USART_WriteByte(NIBP_USART,'-');

}
int main(void)
{
status_t status;
ctimer_config_t configtimer;
ctimer_match_config_t matchConfig;
enet_config_t config;
//uint8_t index;
void *buff;
phy_speed_t speed;
phy_duplex_t duplex;
uint32_t refClock = 50000000;
uint8_t *buffer;
uint32_t timedelay;
bool link=false;

int termWidth;
int termHeight;
int temp=0;
int charWidth;
int lineHeight;
int i=0,j=0;
int c = 0;
int c_prev = 0;
unsigned long errRt=0;
char xyz[10];
WM_HWIN hItem;
int xSize=0,ySize=0;
unsigned int memTest[100];
static unsigned char Toggleled=0;
uint32_t index;



BOARD_InitBootPins();
BOARD_InitBootClocks();
BOARD_InitBootPeripherals();
BOARD_InitSDRAM();

POWER_DisablePD(kPDRUNCFG_PD_USB0_PHY); /*< Turn on USB Phy */
POWER_DisablePD(kPDRUNCFG_PD_USB1_PHY); /*< Turn on USB Phy */

CLOCK_EnableClock(kCLOCK_Gpio4);

/* Enable the RTC 32K Oscillator */
SYSCON->RTCOSCCTRL |= SYSCON_RTCOSCCTRL_EN_MASK;

// For ADC
/* Enable the asynchronous bridge */
SYSCON->ASYNCAPBCTRL = 1;

// Set the back light PWM. Below is not working as Backlight pin is set as permanently high
BOARD_InitPWM();
CLOCK_EnableClock(kCLOCK_Sdio);
//Enable PINT
CLOCK_EnableClock(kCLOCK_Pint); 


BOARD_TestSDRAM();

while(1)
{

}

return 0;
}

/---------------------------------------------------------------end------------------------------------------------------------------------------------------------------

 

 

0 项奖励
回复

4,501 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

So first of all you need make the SDRAM work well.

Do you initialize SDRAM before use?

About SDRAM hardware connection, you can refer to schematic of lpcxpresso54628-evk:

https://www.nxp.com.cn/downloads/en/schematics/LPCXpresso546xx-540xx.zip  

 

 

BR

Alice

0 项奖励
回复

4,491 次查看
nithin3200
Contributor IV

 

Hi  @Alice_Yang,

 

Thanks for the replay.

Yes, I am  initialize SDRAM before use. After cross checking my schematic and lpcxpresso54628-evk.There no difference in hardware.

0 项奖励
回复

4,482 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

How do you initialize SDRAM?

Do you have lpcxpresso54628-evk board? If have, test your simple project on it. 

If no, you can send it to me, I check it on my side.

 

BR

Alice

0 项奖励
回复

4,528 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

Recommend you first using a simple project to confirm the SDRAM can work well,

There is an application note about how to initialize SDRAM :

https://www.nxp.com.cn/docs/en/application-note/AN12423.pdf  

 

BR

Alice

0 项奖励
回复