How to achieve 80MHz using DMA from LPC4370's HSADC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to achieve 80MHz using DMA from LPC4370's HSADC?

31,482 Views
benjaminartes
Contributor I

I am currently trying to help a colleague get use the LPC4370's HSADC for a sensor project and am unable to get the advertised 80M samples from a single ADC channel (ADC0).  We are using LPCXpresso and 2 LPClink2's.  We have based the project off the example code in "periph_hsadc".  We're using some ~2MHz test signals to verify performance (# of samples per cycle).

 

I've thoroughly read through the relevant sections of the Datasheet and User Manual (CGU, HSADC, DMA etc).  I understand the operation of the ADC and it's associated FIFO and also have a good understanding of the DMA settings.  I've reviewed many posts found through google (including every relevant post on here).

Issues:

  • Unable to achieve 80MHz from HSADC.  Using a 2 MHz sine wave and reading for 4095 samples we see ~20 samples per cycle showing that ADC and DMA are, combined, storing 40MHz bandwidth of data.  I assumed this was due to DMA configuration and that ADC was dropping samples due to a full FIFO.  Tried using burst reads from DMA and ending up reading an empty FIFO ~every other sample.  I believe HSADC is currently running at 40MHz even though it reports that it's clock is set to 80MHz.  Code is included below: What could possibly be limiting the sample-rate?
  • As discussed in previous issue we have tried using burst DMA to no avail.  User Manual is pretty clear that you have to use a FIFO LEVEL smaller than 15 so that src burst size and FIFO LEVEL will be the same, but no combination of FIFO LEVEL and src burst has yielded increased performance.  What are the circumstances / settings that DMA bursts will succeed?
  • We have also tried using Packed mode and run into issues.  Packed mode works fine for ~15 samples after which the packed sample is ALWAYS 0.  What are the limitations on using Packed mode?

 

Configuration:

Using Cortex M4 processor clocked at 204MHz.

AHB is set for 204MHz.

HSADC:

80Mhz.

Uses two descriptor entires: Table 0 entry 0 is first run with long match time to allow ADC to stabilize, then swap to Table 1 entry 0 with shortest match time and branch to self.

Uses no interrupts and has a FIFO Level of 15 (thought we have tried many other FIFO Levels, other settings depending).

Uses fastest CRS setting and has DGEC configured for 80MHz operation.

DMA:

Configured for transfer of 4095 samples from FIFO_OUTPUT[0].

Uses src and dst burst size of 1 (whenever we have tried to change burst size DMA ends up reading empty FIFO ~50% of samples).

Doesn't use Linked List.

Tried using DMA as Flow Controller AND HSADC, performance doesn't change.

 

Thanks,

Ben

 

(And sorry for the code below, tried quoting with syntax highlighting and it hid a large number of the lines)

 

#define HSADC_DMA_READ    8

#define DMA_TRANSFER_SIZE 4095 // max. 4095

#define DMA_CH            7

#define NUM_SAMPLE        DMA_TRANSFER_SIZE

uint32_t sample[NUM_SAMPLE];

 

int main(void)

{

       SystemCoreClockUpdate();

       Board_Init();

 

 

       Chip_USB0_Init(); /* Initialize the USB0 PLL to 480 MHz */

       Chip_Clock_SetDivider(CLK_IDIV_A, CLKIN_USBPLL, 2); /* Source DIV_A from USB0PLL, and set divider to 2 (Max div value supported is 4) [IN 480 MHz; OUT 240 MHz */

       Chip_Clock_SetDivider(CLK_IDIV_B, CLKIN_IDIVA, 3); /* Source DIV_B from DIV_A, [IN 240 MHz; OUT 80 MHz */

       Chip_Clock_SetBaseClock(CLK_BASE_ADCHS, CLKIN_IDIVB, true, false); /* Source ADHCS base clock from DIV_B */

 

 

       /////////////////////////////////////////// HSADC settings ////////////////////////////////////////////////////////////////

       LPC_ADCHS->INTS[0].CLR_EN   = 0x7F; // disable interrupt 0

       LPC_ADCHS->INTS[0].CLR_STAT = 0x7F; // clear interrupt status

       while(LPC_ADCHS->INTS[0].STATUS & 0x7D); // wait for status to clear, have to exclude FIFO_EMPTY

 

 

       LPC_ADCHS->INTS[1].CLR_EN   = 0x7F;

       LPC_ADCHS->INTS[1].CLR_STAT = 0x7F;

       while(LPC_ADCHS->INTS[1].STATUS & 0x7D);

 

 

       /* Initialize HSADC */

       LPC_ADCHS->POWER_DOWN = 0;

       LPC_ADCHS->FLUSH = 1;

       Chip_HSADC_Init(LPC_ADCHS);

       LPC_ADCHS->FIFO_CFG      = (15 << 1) /* FIFO_LEVEL*/ | (1) /* PACKED_READ*/;

       LPC_ADCHS->DSCR_STS = 1;

       LPC_ADCHS->DESCRIPTOR[0][0] = (1 << 31) /* UPDATE TABLE*/ | (1 << 24) /* RESET_TIMER*/ | (0 << 22) /* THRESH*/ | (0xA00 << 8) /* MATCH*/ | (0x10 << 6) /* BRANCH*/;

       LPC_ADCHS->DESCRIPTOR[1][0] = (1 << 31) /* UPDATE TABLE*/ | (1 << 24) /* RESET_TIMER*/ | (0 << 22) /* THRESH*/ | (0x01 << 8) /* MATCH*/ | (0x01 << 6) /* BRANCH*/;

 

 

 

 

       LPC_ADCHS->CONFIG        = (0x90 << 6) /* RECOVERY_TIME*/

                                                         | (0 << 5) /* CHANNEL_ID_EN*/

                                                         | (0x01) /* TRIGGER_MASK*/;

       uint8_t DGEC = 0xE;

       LPC_ADCHS->ADC_SPEED     = (DGEC << 16) | (DGEC << 12) | (DGEC << 8) | (DGEC << 4) | (DGEC);

       //Didn't set threshold registers as they aren't used

       LPC_ADCHS->POWER_CONTROL = (1 << 18) /* BGAP*/

                                                                      | (1 << 17) /* POWER*/

                                                                      | (1 << 10) /* DC in ADC0*/

                                                                      | (1 << 4) | (0x4) /* CRS*/;

 

 

       ////////////////////////////////////////////////////// DMA settings ///////////////////////////////////////////////////////////////////

       Chip_GPDMA_Init(LPC_GPDMA);

       LPC_GPDMA->CONFIG =   0x01;

       while( !(LPC_GPDMA->CONFIG & 0x01) );

       /* Clear all DMA interrupt and error flag */

       LPC_GPDMA->INTTCCLEAR = 0xFF; //clears channel terminal count interrupt

       LPC_GPDMA->INTERRCLR = 0xFF; //clears channel error interrupt.

 

 

       LPC_GPDMA->CH[DMA_CH].SRCADDR  =  (uint32_t) &LPC_ADCHS->FIFO_OUTPUT[0];

       LPC_GPDMA->CH[DMA_CH].DESTADDR = ((uint32_t) &sample);

       LPC_GPDMA->CH[DMA_CH].CONTROL  =  (DMA_TRANSFER_SIZE)   // transfer size

 

 

                                                   | (0x0                << 12)  // src burst size

                                                   | (0x0                << 15)  // dst burst size

                                                   | (0x2                << 18)  // src transfer width

                                                   | (0x2                << 21)  // dst transfer width

                                                   | (0x1                << 24)  // src AHB master select

                                                   | (0x0                << 25)  // dst AHB master select

                                                   | (0x0                << 26)  // src increment: 0, src address not increment after each trans

                                                   | (0x1                << 27)  // dst increment: 1, dst address     increment after each trans

                                                   | (0x1                << 31); // terminal count interrupt enable bit: 1, enabled

 

 

       LPC_GPDMA->CH[DMA_CH].CONFIG   =  (0x1                << 0)   // enable bit: 1 enable, 0 disable

                                                | (HSADC_DMA_READ     << 1)   // src peripheral: set to 8   - HSADC

                                                   | (0x0                << 6)   // dst peripheral: no setting - memory

                                                   | (0x6                << 11)  // flow control: peripheral to memory - DMA control

                                                   | (0x1                << 14)  // IE  - interrupt error mask

                                                   | (0x1                << 15)  // ITC - terminal count interrupt mask

                                                   | (0x0                << 16)  // lock: when set, this bit enables locked transfer

                                                   | (0x1                << 18); // Halt: 1, enable DMA requests; 0, ignore further src DMA req

       LPC_GPDMA->CH[DMA_CH].LLI      =  0;

 

 

       ///////////////////////////////////////// start HSADC and GPDMA //////////////////////////////////////////////////////

       Chip_HSADC_SWTrigger(LPC_ADCHS);

       // start DMA

       LPC_GPDMA->CH[DMA_CH].CONFIG = (0x1 << 0); // enable bit, 1 enable, 0 disable

 

 

       //need to add wait for DMA complete

 

 

       for(int i =0; i<4094; i++)

       {

             ;//Issues with DMA interrupt, wait for end of sampling

       }

 

       Chip_HSADC_FlushFIFO(LPC_ADCHS);

       sts = Chip_HSADC_GetFIFOLevel(LPC_ADCHS);

       Chip_HSADC_DeInit(LPC_ADCHS);

       Chip_GPDMA_DeInit(LPC_GPDMA);

 

 

}

*/

Labels (1)
Tags (1)
40 Replies

11,870 Views
a_bet
Contributor IV

So this is how the FIFO looks like in my debugger, as you can see Matlab correctly display the data from the debbuger.
Selection_217.png

I also tried with:

    /*FIFO's and descriptors' setup*/
    LPC_ADCHS->FIFO_CFG      = (15 << 1) /* FIFO_LEVEL*/
           | (1); /* 1 = PACKED_READ ENABLED*/

To increase the FIFO_LEVEL, but nothing changes.

0 Kudos
Reply

11,440 Views
Ray_V
Contributor V

It looks like the FIFO level is the number of samples, not the number of Words in the FIFO, and it would only need 16 locations when READ_PACKED is not enabled.

What frequency are you running the CPU at? this is where CLK_MX_ADCHS and the register AHB clock is derived from, it needs to be fast enough to transfer the results to the FIFO.

Also, according to the data sheet once the FIFO is full if it takes additional measurements it will overwrite the previous contents, so it would be almost impossible to get a clean waveform this way.

You could try using all 8 descriptors from both tables to take 16 samples.

The first descriptor would have 0x9A match value and BRANCH to next descriptor.

the rest would have match value of 0 and branch to next descriptor until the last descriptor of table 0 which would swap tables and branch to first descriptor.

On the second table the last descriptor would HALT after it's processed.

0 Kudos
Reply

11,466 Views
vitaliylivnov
Contributor III

Hi, a_bet

According to the reference manual, you can only connect the second stage of dividers to IDIVA.

2019-10-14.png

Accordingly, you cannot connect 3 dividers in series.

11,443 Views
Ray_V
Contributor V

Good catch, I forgot to look at the datasheet for clock sources. But I think it's the opposite. IDIVA is the only divider that can be connected to other dividers (IDIVA must be the source).

0 Kudos
Reply

11,440 Views
vitaliylivnov
Contributor III

HI, raymundovelarde

That is exactly what I wanted to say. I attach the divider connection diagram, it is easier to understand from it.

2019-10-14 (2).png

11,465 Views
davidgeorge
Contributor III

Hi all.

I have just successfully configured my LPC4370's ADCHS to take 2048 samples at 60 MHz and transfer to SRAM memory using the GPDMA. The trick to getting the ADCHS and GPDMA to work beyond 30 ish MHz is to use the PACKED_READ option in the ADCHS's FIFO_CFG register.

This packs two samples into each 32bit FIFO word so the DMA is now transferring two samples at a time effectively doubling the transfer rate to memory.

If you don't use the PACKED function the DMA will not have enough AHB bus time to transfer 8 samples @ 60 MHz from peripheral to memory and you will loose samples when the FIFO overflows. It you think about it even at 200 MHz its only 2.5x faster than the FIFO is filling and you need to copy 8 samples from peripheral to memory.

I haven't tested at 80 MHz as my clock is not configured to generate fADC of 80 MHz (yet) but I expect the ADCHS and DMA to still function correctly. Assuming your M4_BASE clock is 200 MHz.

Here are a few tips when configuring the ADC and DMA;

  1. DMA Control : SBSIZE Source Burst = 8 (Same as ADCHS FIFO FILL LEVEL)
  2. DMA Control : S = AHB Master 1 (Peripheral)
  3. DMA Control : D = AHB Master 0 (Memeory)
  4. ADCHS FIFO_CFG : FIFO_FILLED Level = 8 (16 samples),
  5. ADCHS FIFO_CFG : PACKED_READ = 1

I triggered my ADC sampling using the SCT CTOUT_0 signal.

I set the DMA to control the number of samples to take (remember DMA transfer size = 1/2 sample size).

To stop the sampling I used the DMA Transfer Complete Interrupt to inject 8 new Table 0 descriptors into the ADCHS that all have the HALT bit set - this will cause the ADCHS to stop running when the descriptors are re-loaded from the double buffered descriptor registers. My original descriptor last entry had the UPDATE_TABLE bit set to make sure it gets reloaded.

My ADCHS descriptor table had 8 entries to take 8 samples from Channel 0, the last descriptor just branched back to the start and repeated. The last descriptor also had UPDATE_TABLE set ready for the end of sampling. To get full speed samples MATCH = 0 and RESET_TIMER = 1.

My Core PLL1 clock rate is 180 Mhz.

My ADCHS Clock is 60 MHz.

Hope this helps!

David.

11,465 Views
diverger
Contributor II

Hi David, is your 'SRAM' the internal one or a external one (on EMC)?

0 Kudos
Reply

11,465 Views
davidgeorge
Contributor III

Hi.

I am using the internal SRAM to store my samples;

Located in SRAM1 (AHB) 0x20000000..

Have had a working, reliable system for a while now with the LPC Clock running at 200MHz, ADCHS Sampling Rate 80Mhz.

I have to say its been a tricky application to get reliably working at fs=80MHz, very little clear documentation from NXP.

David

11,465 Views
a_bet
Contributor IV

Hi David, that's a very good news to me too.
So, are you experiencing dropping samples with your setup? The only other person I spoke to who achieved 80msps had problems with DMA reload time (even using internal SRAM). See HSADC with GPDMA Transfer Dropping Samples at 80MSps 

Regards

Andrea

0 Kudos
Reply

11,465 Views
davidgeorge
Contributor III

Hi Andrea.

I can confirm I can reliably sample at 80MHz to internal SRAM memory without loosing any samples, my system samples an ultrasound signal so any lost samples will be evident and cause a problem.

During sampling there is only the RTOS tick timer running and I halt all other bus transfers, my application code sits in SRAM (0x1000_0000) and sample memory is AHB SRAM (0x2000_0000). CPU clock is 200MHz and I use the Audio PLL to generate the ASCHS Sample Clock.

Because I need to take more than 4096 samples I don't use the DMA to control the ADCHS, instead I load a continuous sample sequence into the ADCHS descriptor table and use TIMER0 to time the sampling process, a TIMER0 interrupt halts sampling by injecting a HALT command into the descriptor table. I could not get DMA Linked Lists to work at fs=80 MHz as once the DMA tries to load the next List the ADCHS overruns its FIFO and the data gets corrupted.

I have also found you must clear the ADCHS FIFO before starting a sampling run otherwise data gets corrupted.

In summary the ADCHS can sample to SRAM at 80MHz but you must;

  1. Use the DMA in burst mode
  2. Set CPU Clock to 200MHz
  3. Halt all other bus transfers during sampling
  4. Use hardware for counting/timing (Timers etc)
  5. Sample to internal AHB SRAM memory
  6. Manage the ADCHS' FIFO correctly
  7. Pack two samples into each 32 bit word ( thanks Ray )

David

10,501 Views
lqlq
Contributor I

May I share your configuration code? I still lose data when I try to configure

0 Kudos
Reply

11,465 Views
a_bet
Contributor IV

Unfortunately I don't have the HW at the moment to try the update right now. By the way, I plan to do it in the next weeks while on holiday. Do you know if using a thrashold-based interrupt on the ADCHS could cause any problem? I need to detect a threshold crossing in my application since I need to acquire and process a pulse shaped signal... at 40 msps it works fine.

0 Kudos
Reply

11,465 Views
Ray_V
Contributor V

Packing 2 samples in one 32-bit read cycle (PACKED_READ (bit0) of ADCHS FIFO_CFG register) allows for 8192 samples. It also improves reliability as the effective transfer rate at 80msps is 25ns instead of 12.5ns

-Ray

0 Kudos
Reply

11,465 Views
davidgeorge
Contributor III

Yes, you're correct, I do pack two samples into each 32bit word.

But I needed more that 4094 "words" in my application hence using a timer.

0 Kudos
Reply

11,465 Views
Ray_V
Contributor V

Do you need all those samples in your application? or do you just need samples after a certain time? (after 120us for example). I am asking because if you don't need the first portion of the waveform you can always set the MATCH_VALUE in the descriptor to start sampling later. For example to start sampling 120us later you can set MATCH_VALUE to 9600  (9600 * 12.5ns) and then collect only the number of samples you actually need.

0 Kudos
Reply

11,465 Views
Ray_V
Contributor V

The LPC4370 ADCHS works well at 80 Msps. As I mentioned in this thread on April, 6 2018  I have it working.

It is reliable and not dropping any samples. Disable interrupts during sampling as any interrupts could cause loss of samples by interfering with the BUS traffic from the DMA. You can check the DMA Interrupt Terminal Count (register INTTCSTAT) to determine when the requested number of samples have been transferred.

Regards,

Ray

11,465 Views
diverger
Contributor II

It's a good news to me. What about DMA to the external SRAM chips? Is it possible?

0 Kudos
Reply

11,465 Views
davidgeorge
Contributor III

As the DMA is used to transfer from ADCHS to a 'memory' address, if that address was external memory connected via the EMC it should work. Obviously your bandwidth will depend on memory speed and configuration, its probably going to be slower than internal SRAM using the AHB Bus.

0 Kudos
Reply

11,465 Views
a_bet
Contributor IV

Hi David, it is great to hear someone who is using this chip and its AD capabilities. I think it's quite underrated!
Right now I'm sampling @40 MHz and I'm fine with that, but still have a lot of questions about this micro (for example see here).
I'd be glad to collaborate if someone needs help and try to help each other.. there's a lack of support and resources (lpcopen support I believe is still incomplete for this chip), but we can join forces:)

Regards,
Andrea

11,465 Views
a_bet
Contributor IV

Hi @benjamin, thanks for posting your code. I'm trying to use it and display some data in Matlab, but I'm having trouble understanding how do you format the data out put. I tried to force the 2 complement format for the ADC but I still get a dynamic range of 2.1475e+09 (which is absurd) and a non sense graph.

I'm just using your code with this little cycle at the end:

for(int i =0; i<4095; i++)

  {

  DEBUGOUT("%04d\r\n",sample[i]);

  }

Let me know if you managed to reach the 80msps, I need to use this HSADC for a thesis and I'm highly interested.
Thanks in advance!

Andrea

0 Kudos
Reply