How to Enable RAM 2 in Keil

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Enable RAM 2 in Keil

1,766件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rezaabdi on Thu Aug 15 08:51:46 MST 2013
HI
I'm going to RAM2 on LPC1768 microcontroller will activate the program KEIL
I want to put a variable in RAM2
If you have information about a friend who can help me
Thank you
ラベル(1)
0 件の賞賛
返信
1 返信

1,587件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Thu Aug 15 10:20:22 MST 2013
By default, IRAM2 should be available in the LPC1768 by selecting this microcontroller in the Device tab of the project.
In order to use IRAM2, you can use the methods described on the Keil website:
http://www.keil.com/support/docs/3357.htm
http://www.keil.com/support/docs/2829.htm
0 件の賞賛
返信