How many PMSM motors can the LPC553x run?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How many PMSM motors can the LPC553x run?

1,677件の閲覧回数
dav1
Contributor V

I've seen the motor demo with the LPC553x. Curious if there has been any tests done on the total qty of  BLDC/PMSM motors on IC could run!?

タグ(3)
0 件の賞賛
返信
1 返信

1,671件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you use LPC553x to control PMSM or BLDC, for each LPC553x,  there are two eFlxPWM modules, two ENC modules(which can decode Encoder signal to get rotor position), two ADC modules, so each LPC553x can control two motors, in other words, the two motors can be  two PMSM,  two BLDC,  or one PMSM and one BLDC.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信