How many PMSM motors can the LPC553x run?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How many PMSM motors can the LPC553x run?

1,709 Views
dav1
Contributor V

I've seen the motor demo with the LPC553x. Curious if there has been any tests done on the total qty of  BLDC/PMSM motors on IC could run!?

Tags (3)
0 Kudos
Reply
1 Reply

1,703 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you use LPC553x to control PMSM or BLDC, for each LPC553x,  there are two eFlxPWM modules, two ENC modules(which can decode Encoder signal to get rotor position), two ADC modules, so each LPC553x can control two motors, in other words, the two motors can be  two PMSM,  two BLDC,  or one PMSM and one BLDC.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply