How many PMSM motors can the LPC553x run?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How many PMSM motors can the LPC553x run?

1,722 次查看
dav1
Contributor V

I've seen the motor demo with the LPC553x. Curious if there has been any tests done on the total qty of  BLDC/PMSM motors on IC could run!?

标记 (3)
0 项奖励
回复
1 回复

1,716 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

If you use LPC553x to control PMSM or BLDC, for each LPC553x,  there are two eFlxPWM modules, two ENC modules(which can decode Encoder signal to get rotor position), two ADC modules, so each LPC553x can control two motors, in other words, the two motors can be  two PMSM,  two BLDC,  or one PMSM and one BLDC.

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复