How do you debug an external target with an LPCXpresso812-MAX board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do you debug an external target with an LPCXpresso812-MAX board?

1,984 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Timur on Sun Apr 17 10:42:31 MST 2016
Hey guys,

We are using the LPC812 (the XSON16 package version) in an upcoming project. So we got an LPCXpresso812-MAX board from Farnell to experiment with it. The website of the board says that it can connect to an external target to debug it, and we've found the debug connector in the documentation on this website.

So far we've tried some basic examples from the LPCOpen package which work on the board wonderfully.

However, it is unclear how to debug an external target with this board. Obviously, I'll need to connect SWDIO, SWCLK, RESET, VDD, GND, etc. of the target board to the LPCXpresso, but how do I tell the LPCXpresso to debug the external target instead of the on-board MCU?

Thanks in advance for your answers!
Labels (1)
0 Kudos
Reply
4 Replies

1,885 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply

1,885 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Mon Apr 18 09:53:21 MST 2016

Quote: Timur
However, it is unclear how to debug an external target with this board. Obviously, I'll need to connect SWDIO, SWCLK, RESET, VDD, GND, etc. of the target board to the LPCXpresso, but how do I tell the LPCXpresso to debug the external target instead of the on-board MCU?



Just separate this lines  :O

This boards are able to debug external targets with their LPC11U35. Unfortunately there are no jumpers to disconnect the LPC812  :((

Anyway, a LPC-Link2 is faster, so it's recommendable to use a Link2  ;-)
0 Kudos
Reply

1,885 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Timur on Mon Apr 18 09:27:21 MST 2016
Thanks for your answer!
If this is the case, please fix the MAX board's website which says that it can do it. We would not have chosen it if we had known that it didn't support this feature.
0 Kudos
Reply

1,885 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Apr 18 00:47:16 MST 2016
The MAX boards were not designed to be used as debug probes to debug other boards. You need either an LPCXpresso V2/V3 board or a standalone LPC-Link2. A good starting point for more details is:

https://www.lpcware.com/LPCXpressoBoards

Regards,
LPCXpresso Support
0 Kudos
Reply