How do I transfer data via ETHERNET

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I transfer data via ETHERNET

1,684件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kevin on Thu Apr 04 10:00:37 MST 2013

I need to make the exchange of information between my development board that is using the LPC1768 and a computer through the "ETHERNET" communication using UDP and SNMP. Since the computer is the CLIENT and the SERVER plate.


Can anyone help me somehow?


Thank you.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,605件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aem.nitin on Tue Nov 04 23:32:00 MST 2014

Quote: kevin

I need to make the exchange of information between my development board that is using the LPC1768 and a computer through the "ETHERNET" communication using UDP and SNMP. Since the computer is the CLIENT and the SERVER plate.


Can anyone help me somehow?


Thank you.





I also need to implement SNMP agent over LPC1768. Can you help me
0 件の賞賛
返信

1,605件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pacman on Tue Apr 16 22:13:26 MST 2013

I haven't tried using ethernet on the LPC1768 yet (but I am going to soon, I believe).


If you provide some more information on what you are doing, what hardware you have available and what you want, you might get some (better) answers.


For instance...


<ul>
<li>Which board are you using ?</li>
<li>Which ethernet PHY is on your board.</li>
<li>Which Ethernet library are you using (LWIP ?)</li>
</ul>

Personally, I would probably try and use some HTTP protocol instead of UDP/SNMP, but if your skills are better than mine, I won't tell you to change your opinion. At least for a start, I'd try using HTTP, as it's easier for tests.


If you haven't already had a look at it, try...


<span class="Apple-style-span" style="font-family: 'Myriad Pro', Helvetica, 'Helvetica Neue', Geneva, Arial, Verdana; font-size: 13px; line-height: normal;">git clone http://git.lpcware.com/lwip_lpc.git</span>


or download <span class="Apple-style-span" style="font-family: 'Myriad Pro', Helvetica, 'Helvetica Neue', Geneva, Arial, Verdana; font-size: 13px; line-height: normal;"><a title="lwip_lpc" href="http://sw.lpcware.com/?p=lwip_lpc.git&a=snapshot&h=HEAD&fmt=zip&f=latest">lwip_lpc</a></span>.

0 件の賞賛
返信