How do I set up and use LPC1347 GPIO pins?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How do I set up and use LPC1347 GPIO pins?

2,225 次查看
injunear
Contributor III

I have been searching for the last three days on how to set up and use GPIO pins for the LPC1347. I have not found how to do it. I have the LPCXpresso board V1 (#OM13045). I have poured over the LPCOpen software and what I find there is too complicated for a non-programmer like me to understand.

I have successfully worked with STM DISCO, Beaglebone Black and Raspberry Pi 3 boards, but I can't find the magic words that let me use the GPIOs of the 1347 board.

Where can I find these most basic of commands, please?

Also, what are the commands in C to write to, and read, from the registers?

Thank you.

标签 (3)
标记 (1)
0 项奖励
回复
2 回复数

1,815 次查看
soledad
NXP Employee
NXP Employee

Hi,

Please check the following document, this is for LPC11u24 however the process is the same for the LPC1347 device.

How to create a new LPC project using LPCOpen and LPCXpresso 

Let me know if this helps!!


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,815 次查看
injunear
Contributor III

The response was a little bit helpful but it did not answer the question.

0 项奖励
回复