How do I enlarge .bin file size, and write data to a specific address?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How do I enlarge .bin file size, and write data to a specific address?

7,404 次查看
at-nakano
Contributor II

Hi,

I'm using LPC4078 with MCUXPresso.

By default, the file size of .bin is smaller than flash size, but I wanted to enlarge file size to 0x80000 (Whole flash), and locate 4-bytes data at 0x7fffc.

Is it possible?

0 项奖励
回复
9 回复数

7,331 次查看
at-nakano
Contributor II

Hi All,

Thank you guys for the answers, it helps a lot.

However, I have not solved the issue to be cleared.

What I wanted to is, put 4 bytes data at very end of bin file, regardless file size.

I did tried # pragma directive like:

#pragma address data_on_eof = 0x2f000

ULONG data_on_eof = 0x0000E1F1;

Note: Current file size is 179,356 bytes (0x2bc9c)

But line "#pragma" was ignored by gcc, and
.data.data_on_eof
0x10000000 0x4 ./src/test/test.o
0x10000000 data_on_eof

Is there any way to locate "data_on_eof" at the very end of .bin file anyway?

Regards,

0 项奖励
回复

7,327 次查看
frank_m
Senior Contributor III

Binary files are not intended for that purpose. They contain no meta information, just plain machine code. Here is a good explanation:https://software-dl.ti.com/ccs/esd/documents/sdto_cgt_an_introduction_to_binary_files.html

Your best option, as suggested, would be to switch to a format containing meta data, namely addresses. Like S19/S-Record, or Intel HEX. This is usually done in the linker settings of your project.

As the given link explains, you can always create a bin file from a S19/HEX file with the objcopy command.

0 项奖励
回复

7,393 次查看
at-nakano
Contributor II

Hi XiangJun Rong

Thank you for your reply.

Right after I posted this question, I was realized that the .bin file is not a flash image, and my question was so stupid...

Anyway, I'll check S-Record as you recommended to, but it is appreciated if you have some information about S-Record.

Thanx.

 

0 项奖励
回复

7,384 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

For the S-Record file format, pls refer to the docs:

http://www.amelek.gda.pl/avr/uisp/srecord.htm

https://en.wikipedia.org/wiki/SREC_(file_format)

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复

7,381 次查看
at-nakano
Contributor II

Hi XiangJun,

Thanks a lot!

Regards,

0 项奖励
回复

7,398 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,Atsuki,

As you know that the *.bin file only contains binary code and data, which does not contain any address, if you want to enlarge the data to 0x8_0000, you have to fill all the hole with data until it reach to 0x8_0000 address.

I suggest you generates S-Record file, which has address information, so you are not required to fill the empty address.

Hope it can help you

BR

XiangJun Rong

标记 (1)
0 项奖励
回复

7,390 次查看
frank_m
Senior Contributor III

> As you know that the *.bin file only contains binary code and data, which does not contain any address, if you want to enlarge the data to 0x8_0000, you have to fill all the hole with data until it reach to 0x8_0000 address.

This should not be necessary.

If one defines variables/data at given addresses, the linker will place it there, and the BIN file will automatically fill up all the gaps.

This is why the question is usually the other way around : "Why is my BIN file so big ?"

The GCC toolchain uses the __attribute__ specifier to modify such features. Check the tutorial for details.

0 项奖励
回复

7,388 次查看
at-nakano
Contributor II

Hi Frank,

Thank you for your reply.

I understand and will check more based on your information.

Thanks a lot!

0 项奖励
回复

7,372 次查看
frank_m
Senior Contributor III

I never tried that with the MCUXpresso toolchain. You might need to to create a special linker section.

The syntax is very toolchain specific, and I did the same thing for the IAR and Keil enviroments a while ago, which use different compilers.

0 项奖励
回复